lpcware

Problems Connecting to VM

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by ewajs on Sun Jun 16 16:33:20 MST 2013
Hi,
I'm currently using a MacBook Pro running OS X (10.8.3) and I have a VM (via Parallels Desktop) running XP SP2 with LPCXpresso 5 on it, whenever I try to debug (on a non modified LPC1769 Kit) I get the same message:
"Premature end of file.:null(line:1, Col:1)"
And see that the VM is not detecting my board.
I'm working with another Windows based computers and had to install the VM because I wasn't able to import the Windows Projects on my LPCXpresso running on OS X (they were FreeRTOS projects).

Parallels Windows detects the board, but not the LPCXpresso on XP SP2. I could initially program the board in the Mac version of LPCXpresso but when I started using freeRTOS i couldn't import existing projects and make them work on the Mac version.

Thanks in advance.

Outcomes