lpcware

crt_emu_cm_redlink commandline parameters and VERIFY option

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by avass on Thu May 07 15:19:04 MST 2015
Hi,

I'm using LPCXpresso v7.5.0 [Build 254] [2014-10-31]  and programming an NXP LPC1115/303's flash from the IDE (Program Flash using LPCLINK2 Redlink).

1. I was looking for an option to "verify flash" after programming, but found none. Is this a no-no?   ( CRP is not set... // CRP_WORD = CRP_NO_CRP )

2. The commandline the current IDE programmer uses is :
    crt_emu_cm_redlink -flash-load "C:\projects\ARM_Code\Release\ARM_Code.axf" -g -2  -vendor=NXP -pLPC1115/303 -flash-driver=LPC11_12_13_64K_8K.cfx

   What is -g  ?
   What is -2  ?

Thanks,

-A

Outcomes