Content originally posted in LPCWare by janderson on Wed Jun 19 08:57:47 MST 2013
Quote: CodeRedSupport
There are two possibilities:
1. You have blown up your target board
2. You have blown up your LPC-Link
I cannot think of anything else.
p.s. as you keep being told, the memory configuration is completely irrelevant until you can actually debug the chip.
I had the LPC1769 target portion resoldered and successfully debugged the Twinkle example program and it is working as it should - looks like this is an issue with the 1850 board.
Also - I have noticed that the display on the screen on the 1850 board is no longer showing up. The demo software used to display a message and display a message when you pushed buttons, moved the jostick, etc, but no longer shows up. HOWEVER, once I moved the BOOT2 jumped into the 1-2 position, the message comes back. Is this ok?
Thanks.