Content originally posted in LPCWare by JDrumm on Fri Apr 16 08:02:20 MST 2010
All,
Thanks for the responses so far. I am trying to use C# to develop my host USB interface to the LPC1343. I have looked at the examples at Jan Axelson's web pages and they are nice, but they only solve the host side of the equation and now the HID example supplied by NXP has to be modified in a way I cannot seem to figure out. I would love to have an example that shows BOTH the host and the target side. If only NXP would publish the source for the host USB code that works with the HID LPC1343 example I would finally have the example I desire.
Thanks,
John