Content originally posted in LPCWare by pikeaero on Sat Mar 05 06:01:52 MST 2011
I Went through the install process (LPCXpresso 3.8.2 Build 129) without a hitch. Imported examples, fine, switch from LPC1114/301 target to LPC1114/302 target, no problems there.
Project builds fine, but when I attempt to debug, cannot connect to emulator board as per the error dialog attached.
Host is an AMD Phenom Quad/64 w/6GB RAM, etc.. Kubuntu Linux 10.10 64-bit Desktop Edition
I am running LPCXpresso as a regular unprivilaged user. I ran the install with root privilages. The install landed in /usr/local/LPCXpresso, the following are setuid root.root:
-rwsr-sr-x 1 root root 112724 2011-01-12 03:36 crt_emu_a7_nxp
-rwsr-sr-x 1 root root 112724 2011-01-12 03:36 crt_emu_a9_nxp
-rwsr-sr-x 1 root root 223732 2011-01-12 03:36 crt_emu_cm3_nxp
-rwsr-sr-x 1 root root 223732 2011-01-12 03:36 crt_emu_lpc11_13_nxp
-rwsr-sr-x 1 root root 22272 2010-05-29 06:36 dfu-util
uname -a is:
Linux pikeaero-desktop 2.6.32-23-generic #37-Ubuntu SMP Fri Jun 11 08:03:28 UTC 2010 x86_64 GNU/Linux
lsusb is:
Bus 006 Device 001: ID 1d6b:0001 Linux Foundation 1.1 root hub
Bus 005 Device 001: ID 1d6b:0001 Linux Foundation 1.1 root hub
Bus 004 Device 002: ID 1a86:7523 Unknown HL-340 USB-Serial adapter
Bus 004 Device 001: ID 1d6b:0001 Linux Foundation 1.1 root hub
Bus 003 Device 001: ID 1d6b:0001 Linux Foundation 1.1 root hub
Bus 002 Device 002: ID 058f:3820 Alcor Micro Corp.
Bus 002 Device 001: ID 1d6b:0001 Linux Foundation 1.1 root hub
Bus 001 Device 011: ID 1fc9:0009
Bus 001 Device 008: ID 05ac:0304 Apple, Inc. Optical USB Mouse [Mitsumi]
Bus 001 Device 006: ID 067b:2303 Prolific Technology, Inc. PL2303 Serial Port
Bus 001 Device 005: ID 0c76:1607 JMTek, LLC.
Bus 001 Device 002: ID 05e3:0605 Genesys Logic, Inc. USB 2.0 Hub [ednet]
Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
Looks the like the LPCExpresso is USB Device "1fc9:0009" but is not recognized? Is there a kernel device loadable module for it? Or what gives here?
--Mike