Content originally posted in LPCWare by lpcxpresso-support on Wed Jan 08 08:57:31 MST 2014
Debugging a "hello world" program created using the LPC17 project wizard seems to work fine here on an mbed board connected via CMSIS-DAP.
I wonder if this is somehow image related. Can you try creating a test project using the project wizard and seeing if that debugs correctly?
If you still see problems, it might also be worth trying a mass erase of the flash before you program:
Also can you confirm which platform you are using. I presume Windows from the debug log - but XP, 7, 8 and 32 or 64 bit?
Regards,
LPCXpresso Support