lpcware

Download large firmwares

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by ngoncalves on Wed Feb 22 15:37:21 MST 2012
Hi,

Probably this was answered before but I could not find it anywhere.

I have CodeRed IDE with limited to 128K download size. My firmware, in   itself is less than 50K, but the processor (LPC1758) has 512K of flash.

Since we have a lot of free space in the flash of the processor, we want to use it to store the firmware of another processor, which can only execute from RAM. The idea is allocate a chunk of the LPC1758 flash to the firmware, and download after power-on to the other processor.

The problem is that the firmware image is 190K. Is there a way to download 190K using the debugger that comes with the LPCXpresso ?

Thanks

Outcomes