C:\nxp\LPCXpresso_6.1.0_164\lpcxpresso\tools\bin\arm-none-eabi-gdb.exe test.axf |
target extended-remote | C:/nxp/LPCXpresso_6.1.0_164/lpcxpresso/bin/crt_emu_cm3_nxp.exe -g -2 -pLPC1769 -wire=hid set remotetimeout 60000 set arm force-mode thumb load monitor semihosting enable continue |
C:\nxp\LPCXpresso_6.1.0_164\lpcxpresso\tools\bin\arm-none-eabi-gdb.exe test.axf GNU gdb (GNU Tools for ARM Embedded Processors) 7.3.1.20121016-cvs Copyright (C) 2011 Free Software Foundation, Inc. License GPLv3+: GNU GPL version 3 or later <http://gnu.org/licenses/gpl.html> This is free software: you are free to change and redistribute it. There is NO WARRANTY, to the extent permitted by law. Type "show copying" and "show warranty" for details. This GDB was configured as "--host=i586-mingw32 --target=arm-none-eabi". For bug reporting instructions, please see: <http://www.gnu.org/software/gdb/bugs/>... Reading symbols from test.axf...done. Ni: LPCXpresso Debug Driver v6.0 (Oct 16 2013 02:04:27 - crt_emu_cm3_nxp.exe bui ld 1212) Pc: ( 0) Reading remote configuration Nc: Looked for chip XML file in C:/nxp/LPCXpresso_6.1.0_164/lpcxpresso/bin/LPC17 69.xml Nc: Looked for vendor directory XML file in C:/nxp/LPCXpresso_6.1.0_164/lpcxpres so/bin/nxp_directory.xml Nc: Found generic directory XML file in C:/nxp/LPCXpresso_6.1.0_164/lpcxpresso/b in/crt_directory.xml Pc: ( 5) Remote configuration complete Pc: ( 30) Emulator Connected Pc: ( 40) Debug Halt Pc: ( 50) CPU ID Nc: Emu(0): Conn&Reset. DpID: 2BA01477. Info: HID64HS12 Nc: SWD Frequency: 3000 KHz. RTCK: False. Vector catch: False. Nc: Packet delay: 0 Poll delay: 0. Nc: Loaded LPC175x_6x_512.cfx: LPC175x_6x (512K) Apr 22 2013 12:14:31 On-chip F lash Memory Nc: NXP: LPC1769 Part ID: 0x00000000 Pc: ( 65) Chip Setup Complete Nt: Connected: was_reset=false. was_stopped=true Cr:v LPCXpresso Free License - Download limit is 256K Pc: ( 70) License Check Complete Pc: ( 85) Registered Semihost Handler Pc: (100) Target Ready main () at ../src/main.c:27 27 uint32_t i=0; Loading section .text, size 0x2c48 lma 0x0 Nt: Writing 11336 bytes to 0000 in Flash (assumed clock: 4.0MHz) Pb: 1 of 1 ( 0) Writing pages 0-2 at 0x00000000 with 11336 bytes Ps: ( 0) Page 0 at 00000000 Ps: ( 0) Page 0 at 00000000: 4096 bytes Ps: ( 36) Page 1 at 00001000: 4096 bytes Ps: ( 72) Page 2 at 00002000: 3144 bytes Nt: Erased/Wrote page 0-2 with 11336 bytes in 1636msec Pb: (100) Finished writing Flash successfully. Nt: Flash write Done Nc: nSRST assert (if available) Nc: Executing in user flash. Nt: Start address 0x129, load size 11336 Transfer rate: 3 KB/sec, 11336 bytes/write. Semihosting enabled. |
set mem inaccessible-by-default off |