Content originally posted in LPCWare by Kaare on Tue Jul 12 05:29:42 MST 2011
Hi
I have just installed the LPCXpresso V4.05, and trying to get the Blinky example for the LPC1114/302 board up and running.
But when I try to start the debugger, I get the following error:
[I]No emulator or board available.
This could be because it is unpowered, unconnected or already in use[/I]
I have connected the Expresso board to my PC, and there is power on the module.
I made the default install when I first connected the board to the PC.
I cannot find any information that i should install another driver?
I have tried to change some settings for the debugger interface, but nothing helps.
Please help! Why does this not work right out of the box?
Thanks
Kaare