Content originally posted in LPCWare by exgreyfox on Mon Jul 01 14:45:59 MST 2013
Hello gents,
I am having an issue with a hard fault in my code. Basically I have some code written up that will talk to a DAC via SPI and spit out a voltage profile (0-2.5v) and what I am trying to do is read that voltage back into the ADC input channel 0 and have it be displayed by the debugger using printf. To do this i just re-used the code from the adc example. I'm getting a hard fault as soon as I start the debugger. I'm attaching my project below. Any help is greatly appreciated.