Content originally posted in LPCWare by m2babaey on Mon Jul 01 05:24:04 MST 2013
I looked at my supply voltage by oscilloscope and there was 500mV AC on my 3.3V Although I had 10 x100nF capacitors on the chip
I added an electrolytic capacitor and now my circuit starts working even when I have 100nF capacitor on reset pin
Just there is one more problem. I have a switch that connects reset pin to GND. When I apply a low to the reset pin, the chip stops and doesn't restart when I remove the low level on the reset pin
I looked at the links, maybe the chip is entering ISP mode. but I have a 10K pull up resistor on P2.10. what else should I do?
This is interesting that when jtag connector is connected to the board, the reset switch works fine and the CPU restarts normally after reset