lpcware

Configure LPCXpresso to use semihosting

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by xjx on Thu Nov 05 17:28:46 MST 2015
Hello All,

I need to add semihosting capability to a project. I read the following note:

http://www.support.code-red-tech.com/CodeRedWiki/UsingPrintf

so I followed this steps:

1)  "Project -> Properties".
2) In the left-hand list of the Properties window, open "C/C++ Build" and select "Settings" and then the "Tool Settings" tab.
3) Choose "MCU Linker - Target"
4) In "Use C library" field, select either "Redlib (semihost)" or "Newlib (semihost)"

However, I can not do step 4. Could you please help?

I attach some related images.

thank you!!!


Outcomes