Content originally posted in LPCWare by tecnosys on Sun May 09 16:56:47 MST 2010 I want to put the mini 10pin JTAG/SWD on a prototype board with the LPC1768 for use with the LPC-Link. Should I connect pin 7? See Keils Pinout vs my schematic, is this used. Or do I leave it disconnected?
Content originally posted in LPCWare by finfo on Tue May 18 13:25:32 MST 2010 The same question as with the LPC236x series. Just I don't have the Pinout I would need.
Content originally posted in LPCWare by NXP_USA on Tue May 11 14:25:01 MST 2010 Quote: tecnosys I want to put the mini 10pin JTAG/SWD on a prototype board with the LPC1768 for use with the LPC-Link. Should I connect pin 7? See Keils Pinout vs my schematic, is this used. Or do I leave it disconnected?
It is best not to connect pin 7. Pin 7 is a key pin which should be removed from the connector. Pin 7 on the cable should be filled in. This prevents the connector from being inserted backwards. We recommend adding a pin 1 indicator on your board in case the cable is not keyed.