Content originally posted in LPCWare by askar on Thu May 29 23:59:19 MST 2014
Hi,
for creating multi core application for lpc4357,
in Free edition of lpcxpresso version 7.0.0, first i created a project for m0
then i created project for m4 and set the loading address for m0 to be flash2.
i compiled m0 without any error, then compiled m4 and there was
"M0APP execute address differs from address provided in source image" i checked mcu setting in m0 and saw that
flash driver is set to bank A, i tried many times to set flash driver to bank B but with no success.
any help is appreciated in advance.
best regards,