// ********************************************************************* // Define the IP address to be used for the MCU running the TCP/IP stack // ********************************************************************* [COLOR=Red]#define MYIP_1 192 #define MYIP_2 168 #define MYIP_3 0 #define MYIP_4 100[/COLOR] |
/** * Specifies if the uIP ARP module should be compiled with a fixed * Ethernet MAC address or not. * * If this configuration option is 0, the macro uip_setethaddr() can * be used to specify the Ethernet address at run-time. * * \hideinitializer */ #define UIP_FIXEDETHADDR 1 #define [COLOR=Red]UIP_ETHADDR0 0x00[/COLOR] /**< The first octet of the Ethernet address if UIP_FIXEDETHADDR is 1. \hideinitializer */ #define [COLOR=Red]UIP_ETHADDR1 0xFF[/COLOR] /**< The second octet of the Ethernet address if UIP_FIXEDETHADDR is 1. \hideinitializer */ #define [COLOR=Red]UIP_ETHADDR2 0xFF [/COLOR] /**< The third octet of the Ethernet address if UIP_FIXEDETHADDR is 1. \hideinitializer */ #define [COLOR=Red]UIP_ETHADDR3 0xFF[/COLOR] /**< The fourth octet of the Ethernet address if UIP_FIXEDETHADDR is 1. \hideinitializer */ #define [COLOR=Red]UIP_ETHADDR4 0xFF[/COLOR] /**< The fifth octet of the Ethernet address if UIP_FIXEDETHADDR is 1. \hideinitializer */ #define [COLOR=Red]UIP_ETHADDR5 0xFF[/COLOR] /**< The sixth octet of the Ethernet address if UIP_FIXEDETHADDR is 1. \hideinitializer */ |