Content originally posted in LPCWare by ronkrem on Sun Aug 09 18:55:59 MST 2015
I just upgraded to W10 and have several problems, one of which concerns LPCXpresso. Compiling a program that was working under W8.1 produces this message:
11:43:53 **** Build of configuration Debug for project E300C_USB ****
make -r all
0 [main] us 0 init_cheap: VirtualAlloc pointer is null, Win32 error 487
AllocationBase 0x0, BaseAddress 0x71110000, RegionSize 0x4D0000, State 0x10000
C:\nxp\LPCXpresso_7.9.0_455\lpcxpresso\msys\bin\make.exe: *** Couldn't reserve space for cygwin's heap, Win32 error 0
11:43:53 Build Finished (took 97ms)
The install of v7.9.0_455 was performed under W10 and seemed to have no problems. Any suggestions welcome.