lpcware

Linux software to talk to the boot loader ?

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by ataru on Thu Dec 02 17:23:40 MST 2010
LPC11C14 connected to a Linux host system through the serial port. Application: CAN to serial bridge.

For ease of production and field updates, we would like to program the device in-circuit, using the serial port and the built-in boot loader.

The controller should always go into boot loader first, then the application running on the Linux host can decide whether it needs to update the firmware, or start the flash code on the LPC11C14.

Is there any canned Linux code for this that we can adapt ? I would rather not reinvent this wheel...

Outcomes