I think I need the lpc1768 to act as a device and then connect the usb b to a cable to pc
I gotta take the analog input and send the digital signal to pc through the usb D+ and D- the lpc1768 need to be the device right? and then the pc is the host?
do I need resistors on the D+ and D-
And will the pc now power the lpc1768 by the new breakout board I am adding..
If I connect positive to vout and negative to vin while this breakout board b is connected my pc by the usb cable will it then power the lpc1768...and will it draw just 3.3v or will it draw 5v
I must now cut the tracks of the lpc link and use it as a debugger?
My project is to turn the lpc1768xpresso into a usb audio device