lpcware

Unable to import lpc_board_nxp_lpcxpresso_11u68 + chip level file

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by rc51 on Wed May 28 13:39:22 MST 2014
Hello,

I installed the latest version of LPCXpresso and trying to create a simple blinky project. 

Whether I start w/the "New Project" or "Import project(s)" link in the Quickstart Menu - I am not able to select the following files/libraries

lpc_board_nxp_lpcxpressor_11u68 or lpc_chip_11u6x

They are greyed out and the message states that these are unable to be imported because they already exist in the workspace.  However, they do not exist and I am unable to compile the simply blinky program.  I have tried deleting the files associated with the workspace - even reinstalled LPCXpresso from the website and I am not able to import these files into a workspace.

It may be I am doing something very dumb here but if anyone can guide me, I certainly appreciate it.

Thank you.

Outcomes