lpcware

Easyweb with FreeRTOS on LPC1769

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by kvanderkamp on Wed Dec 05 18:36:22 MST 2012
For a project I'm trying to combine TCP funcitonality with multiple thread support, specifically by combining easyweb with the FreeRTOS example code. Somehow if I add a breakpoint in the Init_EthMAC function just after it sets the PHY to autonegotiation link speed, the code runs well and I'm able to access the webserver. However if I remove the breakpoint it will throw a HardFault.

Does anyone have a suggestion how to fix this, or even an alternative way of adding IP functionality to FreeRTOS?

Outcomes