lpcware

LPC Link failed to connect

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by Prithvi on Wed Dec 01 14:34:28 MST 2010
Hi everyone,
I was working on the the lpcxpresso 1343 board with it powering few leds and a MAX3232 level converter and everything was fine. This was in Vista SP2. And the next day I start again and I start getting the message saying:
"02: Failed on connect: Em(01). Cannot find selected MEM-AP (check target power):" I've attached the message pic.
I then installed lpc xpresso in XP. The DFU drivers were loaded sucessfully and the device was sucessfully recognized as a USB DFU device. But then debugging in lpcxpresso again gave the same message.

What could be the problem? Did I draw too much current and spoil the lpc1343?

Thanks in advance,
Prithvi

Outcomes