USB on-chip driver for the LPC1850, LPC11U24 and the LPC1347

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB on-chip driver for the LPC1850, LPC11U24 and the LPC1347

392 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by halhertani on Thu Apr 26 05:25:53 MST 2012
Hello,
I'm really thrilled with the new on-chip USB library which can be found in the LPC11U24 and the LPC1850 and hopefully in the LPC1347 once its released. Unlike the on-chip USB library in the LPC1343, this newer one can be used to develop CDC, HID, DFU, MSC and custom USB devices (more than one class). With this much functionality one expects the newer on-chip USB library to be more complicated as it indeed is. Also I realize that  Examples exist for the newer  on-chip USB library in the LPC18xx peripheral library.

But it would be nice to publish an appnote on how the new library can be used or provide a tutorial; especially with NXP heavily marketing this kind of functionality.

I'm really excited about the LPC1347 and hope that NXP will release a 128KB Flash / 16KB RAM part in the LPC134x family soon (and possibly with two UARTS!) !!!
0 Kudos
3 Replies

289 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Tue Jun 12 09:42:59 MST 2012
Have you seen this thread:
http://knowledgebase.nxp.com/showthread.php?t=3295
Including this post:
http://knowledgebase.nxp.com/showpost.php?p=17027&postcount=12
0 Kudos

289 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CC58 on Tue Jun 12 09:26:44 MST 2012
I'd be happy if I could just get the LPC1343 on-board USB bootloader to work. I've tried everything in the manual. Still PC will not recognize it as USB device. Got any ideas?
0 Kudos

289 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Europe on Fri May 04 06:51:39 MST 2012
Hi,

Hope you will find following link interesting:
http://www.lpcware.com/content/project/nxpusblib
0 Kudos