lpcware

Can't Disassemble Unless Extension is .axf (or .o)

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by MikeSimmonds on Tue Apr 17 21:12:33 MST 2012
LPCXpresso Windows 4.2.2 275 (the new one).

In project properties (Settings/Build Artifact) I change the extension from .axf to .elf (because that IS what they are!). This is required due to external utilities (developed for previous ARM9 based development projects) that need to be used for our systems.

However, when this is done, the Binary Utilites options are all greyed out!

Where can I add ".elf" to the list of extensions that allow binary utilities?
And why oh why is this not enabled as a default? -- Not everyone uses Keil.

Outcomes