Content originally posted in LPCWare by trioflex on Sat Feb 06 05:17:21 MST 2010
Quote: CodeRedSupport
Hello,
This shows that the firmware loaded correctly, but the LPXCpresso IDE has not detected that the LPC-Link has booted. This could be because the IDE is timing out before the Windows has loaded the drivers.
Can you tell me which OS you are running (XP/Vista/Win7)? Also, are you running on a VM?
After you get this message, can you look at the Device Manager:
If you are running WindowsXP, you should see a USB device called "LPC-Link Debug Probe"
If you are running Window Vista/Win7, you will see an additional HID Device.
If these apeear, try Debugging your application again.
Thanks
I did say in first post that I am using WinXP
and no, i am not running in VM but plain normal WinXP
there LPC-link entry DOES appear in device manager but
it is flagged as having error and the lpc-link drivers are not loaded
i told that already..
"LPC-Link Debug Probe"
this DOES appear, but it is is not enabled as actual drivers
do not get loaded