Content originally posted in LPCWare by Terje on Thu Apr 19 23:26:25 MST 2012
[FONT=Calibri]I have onlytested this using Master Receiver mode. I use the LPCXpresso dev. Kit LPC1343 connected to NSE-5310 position sensor. I have used an oscilloscope only to check for noise and the state of the SCL line before timeout. I have only tested this using normal mode. (The NSE-5310 does not support fast mode). I don't know what you mean by baseboard, but I am using the JTAG interface on the dev kit, if that is what you mean.[/FONT]
[FONT=Calibri]From fig 35 in the manual one can see that status code 58 is triggered as the last action before ending transmission.Placing a breakpoint in this routine, one will find that this case is not always executed.[/FONT]
[FONT=Calibri]My code is now running as expected.[/FONT]
[FONT=Calibri]Rob: Thanks for the link!![/FONT]