Content originally posted in LPCWare by CodeRedSupport on Wed Feb 10 01:46:31 MST 2010
You didn't mention which LPC1768 board you attempted to load the RDB1768_LedFlash project to. The LedFlash application was created for the Code Red RDB1768 evaluation board.
With regard to the error message, the initialization seems to have proceeded to the point the DpID/CPUID/ROM table were validated, the part has halted, and we can connect to the AP bus.
The operation which generates the error message is an attempt by the debug driver to download an IAP interface routine to read out the Part ID. The driver interface has failed to initialize. Did you modify any part of the LedFlash application, the clock/PLL setup in particular?
Regards,
CodeRedSupport
Quote: mturpin
Hello All!
I was using the LPCXpresso board and after testing some programs (Blinky, etc) I separated the LPC-Link board and tried to debug a program on my own (LPC1768) target board through the JTAG interface.
It worked once with the RDB1768_LedFlash. The second time I tried I got the "03: Failed on chip setup: Et: Flash driver not ready." Now it is the same thing every time I try to start debugging.
Any suggestions?
Thanks!