lpcware

LPC1317 external memory interface

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by aamir ali on Tue Apr 30 04:01:04 MST 2013
I am using LPC1317 for one of my project & I am falling short of flash as project is bigger. Now changing controller is difficult.
Can I store code in some external memory & then call it. I have still 5K of Ram left-> 3K in SRAM0 & 2K in SRAM1


I have external SDHC card interface with SPI interface with 18Mhz. Can it help in any way, or any other memory interface to solve the issue.
OR
Any pin to pin compatible NXP series MCU

I am running my system at 72Mhz/3.3V.


CRITICAL FOR MY APP:

Outcomes