lpcware

IDE 5.1.2 Sudden debug problem

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by MikeSimmonds on Thu Apr 18 01:57:04 MST 2013
[FONT=Tahoma][SIZE=2]Suddenly, after 5 or 6 debug starts/stops (IDE continuoulsy open) I get the following error.
Error in final launch sequence
Cannot start StubMsgServer service: ImageRegistry key already in use: lpcxpresso_16x16
This is an extremely usless message for the end user (I'm sure it is clarity itself to Code Red).

So: What does this mean? I.e. why is this key in use (I checked and the debug processes are NOT still running)? How shall it be 'released'.

Obviously, I will try closing and re-opening the IDE, but I think we are entitled to an answer to this.

BTW: I have been given to understand the LPCXpresso does not use the registry.

Also, this is XP Pro/SP3.

[/SIZE][/FONT]

Outcomes