Content originally posted in LPCWare by jdurand on Fri Sep 20 14:35:49 MST 2013
A client built several for his people and gave me one.
I also have one from Zero Computer that adapts to some other cable sizes such as 2mm hard metric.
On the link board, yes, it's a bare board but also is slower in debugging (unless they've updated them) and you have to use that fragile ARM 10 pin header after you cut off the right hand part of the board (or at least cut the traces to it). If it saves me 2-3 hours of time over the life of the debugger, it's worth it for me to buy the "real" one.
So, you can probably get by using the link board, but if it's something you're using all the time the more rugged Red Probe is probably the better deal. I haven't looked at the price recently, but I remember this wasn't all that expensive.
Which reminds me, I've got a couple of Keil debugger pods to put on eBay.