lpcware

lpcxpresso lpc-link supported by IAR!!!

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by Konstantin Salavatov on Fri Dec 02 01:26:51 MST 2011
But unfortunately somebody decided to allow only Chinese developers to use IAR for development with LPCEXPRESSO - UNFAIR GAME!!!

use Google translate to read:
http://www.iartools.com/ProductShow.asp?ClassId=4&Id=379&s0=6&s1=11

«NXP LPCXPresso-CN (that is, NXP LPCXpresso Chinese version) is NXP co-operation with the IAR, [B]for the Chinese market entry[/B] of a development tool, which is based LPC1114 chip ( ARM Cortex-M0 core) design, simulate the circuit with the target set for the whole circuit , with the IAR Embedded Workbench for ARM integrated development environment, is an engineer design is based on Cortex-M0 ‘s the best choice for embedded applications. This product by NXP and its agency distribution channel in China, do not be sold separately.»

Then even give IAR for FREE!!! with LPCExpresso:

«According to IAR and NXP 's agreement, in mainland China, each LPCXpresso-CN development board will allow its users a [B]free upgrade IAR Embedded Workbench[/B] for ARM Learning Edition License Key once, so that IAR Embedded Workbench for ARM compiler CM0 application on behalf of the code limit from 8K to relax for the 32K»

Sincerely,
Konstantin Salavatov,
Unisoft plus

Outcomes