lpcware

LPCXpresso 1769 and Mbed baseboard.

Discussion created by lpcware Employee on Jun 15, 2016
Content originally posted in LPCWare by gvivekcbe on Sat Mar 28 18:46:00 MST 2015
I have got LPC Xpresso 1769 mounted on a mbed-xpresso baseboard.

I am a newbie when it comes to MCU software development. I want to learn freertos, cmsis and peripheral driver development.

1) Could this baseboard be used along with LPC Xpresso 1769?
2) The baseboard webpage has some "stamp" source code for 1768. link
Can I simply compile these source code for target device 1769 and load it?
3) Also I got the source code examples from LPCOpen for 1769. The readme.txt for these examples has some jumper settings for a different baseboard by Embedded Artists. How can I load these samples with the correct jumper settings for the baseboard that I have? I am not able to figure what the jumper configurations are, for this baseboard.

Thanks

Outcomes