Content originally posted in LPCWare by gibsodo on Fri Jun 06 04:11:27 MST 2014
Hello,
we are running LPCXpresso on an Jenkins buildserver. After upgrading from the CodeRed IDE to LPCXpresso 7.1.2 the console output of the build process is not shown.
We are calling LPCXpresso from an Windows batch file with the following parameters:
%LPC_PATH% --launcher.suppressErrors -consoleLog -nosplash -application org.eclipse.cdt.managedbuilder.core.headlessbuild -cleanBuild %CDT_PROJECT%/%CDT_TARGET% -data %WORKSPACE% -vmargs -Dorg.eclipse.cdt.core.console=org.eclipse.cdt.core.systemConsole -Xms40m -Xmx800m -XX:MaxPermSize=256m
I think the error migth be with the -Dorg.eclipse.cdt.console option.
We called the CodeRed IDE with the same options and it worked.