Content originally posted in LPCWare by teslabox on Fri Feb 17 07:08:16 MST 2012
[B]Hello,[/B]
Quote: Zero
If your bus is already terminated, you have to reduce this termination (= solder out this 2 * 60 Ohm resistors)
Yes, it is already terminated because it is a CAN bus in a new brand car working at 125 kpbs.
Now I'm using an mbest board EM-LPC1700 with a LPC1768. I tried to comunicate this evalboard with CAN King KVASER and everything is work properly.
On the EM-LPC1700 evalboard there are two CAN channels. I only use the second one. I saw that there are two 51 Ohm terminator resistors [I](R40 and R41)[/I] as shown on the schematic[I] (look at the attachement: embest EM-LPC1700 Schematic.pdf in ZIP file, page 5, DB9_COM J6, top left corner of the sheetpaper)[/I]. I soldered them out and it still doesn't work porperly in the car and CAN King KVASER shown a "FrameError".
Also when I connect it [I](without R40 and R41 resistors)[/I] to the CAN King KVASER then the "FrameError" occurs during when I send or receive a message from or to CAN King KVASER.
Now I made a socket from universal 2.54 mm Berg goldpins and I can connect or disconnect terminators[I] (two 100 Ohm resistors)[/I] very fast to check the differences. And if I only remove them from the socket I get "FrameError".