lpcware

How to unlock files

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by daniel on Wed Dec 14 12:03:48 MST 2011
I want to play a little bit with the examples from NXP.

What I want is to put a delay in the "can"-example (with timer32.h)
But it still works in the "blinky"-example, but I can't manage it in the "can"-example.

I think the problem is still in the header files, which are gray (see below).

I tried to create a new project with the files of "blinky" and the src file of "can" but it gave the same problem.

I have no idea how to unlock those files.

[IMG]http://www.appelbanaan.nl/Share/NXP-problem.PNG[/IMG]

Outcomes