Content originally posted in LPCWare by lenguyen on Wed Feb 19 08:57:53 MST 2014
Hello,
we create a workspace with a project using board 4078 library. This workspace is under c:\workspace folder. In this workspace there are two project, first is for board library with include all board and chip library under c:\ncp\lpcopen\.... and second is test which is using board library. Everything compile and link OK. Then we decided to move whole workspace to under a folder c:\project\... then there is problem when we recompile the project. it complains about build error. Here's an error:
* Make: *** No rule to make targe `C:/project/nxp/lpcopen/software/lpc_core/lpc_ip/acmp_001.c', needed by `ip/acmp_001.o. Stop.
Any body has the same problem ?
Thank you for your input.
Thanks
ln