Content originally posted in LPCWare by mayur.p.85 on Thu May 09 06:29:30 MST 2013
Hi Guys,
I am trying to use ported uCOS-III on the LPC1769 MCU with LPCExpresso board.When I created a debug image of it, I found that the debug version of axf file size is 2,353KB (I could try with release image too), while from the specification of LPC1769, I found that it has only a flash memory of 512KB on-chip, So Can anybody guide me that what shall be done to achieve uCOS-III flashed in it.
I would like to actually add an External ROM in addition so that I can use internal and external both for flashing. Please also advice me if possible with small information of External ROMs too which I could use with this MCU.
Regards,
Mayur