Content originally posted in LPCWare by jnd on Sat Feb 27 20:39:33 MST 2010
Hi,
I'm runing latest LPCXpresso 3.2.3 (about dialog shows only 3.2.2 but everywhere else it's 3.2.3) under Virtualbox on Linux host. Display license type and Product information shows me FULL license. But when I try to debug larger example like the adc I get errors shown in attachments.
When I try small projects like blinky or systick it works fine and I can debug it, so debugging works well under Virtualbox. I only have to manually disconnect the unknown device and connect LPC-Link Probe at the first LPC-Link initialization.
I guess this has to be something with Windows XP running under Virtualbox. I tried exactly same installation with other machine and native Windows XP where it worked without problems. Is there any way to check where could be problem?