lpcware

Accessing the SD card

Discussion created by lpcware Employee on Jun 15, 2016
Content originally posted in LPCWare by Ajay Thallapalli on Wed Apr 08 04:05:09 MST 2015
Hi,

I am using NGX LPC4330 board for my project and I am programming the board by using DFU Programmer.
Could any one have how to access(to see the complete memory., read as well as write) SD card I got two programs

[color=#306]1.lpcopen_2_12_keil_iar_ngx_xplorer_4330\applications\lpc18xx_43xx\keil_uvision_projects\ngx_xplorer_4330\periph\periph_sdmmc[/color]
[color=#393]2.lpcopen_2_12_keil_iar_ngx_xplorer_4330\applications\lpc18xx_43xx\keil_uvision_projects\ngx_xplorer_4330\misc\sdmmc_speed [/color]

1st program i can able to run and work, but 2nd program i can't understand and it is having some problem, while programming it to NGX board using DFU programmer it is showing an error also.

Could any one tell me the solution.
If any one having SD card program (SPIFI mode) please guide me with the program.

Thanking you.

Outcomes