Content originally posted in LPCWare by pavan_munavalli on Thu Jan 29 07:59:48 MST 2015
Hello all,
I am stuck in a weird problem.
I am programming a CAN application. The stand alone CAN program (which is based on the example program in the LPCopen) works perfectly fine, even after a power restart.
Now I have included the same CAN application into the RTX(based on CMSIS rtos). The application works fine, but does not work after a power restart. Also, the CAN with RTX runs only after running the CAN standalone application which works pretty well.
I have just included the CAN standalone application into a single thread and nothing more.
Can you guys give me an idea where I might have the problem ?
Thanks,
Pavan.