Content originally posted in LPCWare by RA1981 on Tue Jun 07 04:45:37 MST 2011
Hi CodeRedSupport,
Quote:
It appears that the library object containing __aebi_fadd() has been built with the debug information enabled (whereas we would normally remove the debug information from the C library). Thus the debugger tries to display the source - which doesn't exist in your system (as we don't provide the library sources).
Ah, okay, so I didn't make anything wrong :)
Quote:
There are two simple workarounds here - use the "step over" rather than "step in" operation when you step the return statement. Or else if you end up with the error you are seeing in the debugger, then simply click "step out".
Okay, I'll use 'step over' when stepping through single instructions.
Quote:
Anyway, sorry for the confusion this has caused you. This issue will be resolved in the next LPCXPresso release.
No problem, glad to help finding issues and improving products ;)
Regards,
Ralf