Content originally posted in LPCWare by jdurand on Wed Oct 03 15:30:09 MST 2012 I updated LPCXpresso from 4.2.3 to 4.3.0 and started getting errors on it not finding libraries.
I looked at the Includes and see it's got the built-in libraries for BOTH 4.2.3 and 4.3.0 listed. I haven't been able to find where to kill the old built-in libraries yet.
Content originally posted in LPCWare by TheFallGuy on Sat Oct 13 06:58:20 MST 2012 That is the problem. As I said, Workspaces cannot be shared. If you want to develop in two platforms, you will need to use a version control system and check-in/check-out projects (and not workspaces). This is just a fact of life with Eclipse-based IDEs
Content originally posted in LPCWare by jdurand on Sat Oct 13 06:47:50 MST 2012 Just a regular SAMBA share, but the paths that are being added for the LPCXpresso libraries like /usr/local/lpcxpresso_4.3.0_1025 cause error flags on the Windows system and the c:\ stuff upsets the Linux system.
Content originally posted in LPCWare by TheFallGuy on Sat Oct 13 04:17:26 MST 2012 How are you sharing your projects between Linux and Windows? We use Subclipse (subversion) and can share projects without any issues like you describe. You can also share by import/export *projects* but you cannot share workspaces.
Content originally posted in LPCWare by jdurand on Fri Oct 12 14:51:07 MST 2012 I found I just can't go back and forth between Windows and Linux with this software, I have to clear the Discovery paths every time I switch systems. I have to do BOTH "per language" in each project and "Configuration-wide".
As I work on 4 different computers I think I'll just avoid the one Windows one and stay on Linux (now updated all systems to Ubuntu 12.04LTS and broke the activation, but that's now fixed).
Content originally posted in LPCWare by TheFallGuy on Thu Oct 04 00:11:18 MST 2012 How did you update? The official way is to uninstall your existing version and install to a new directory. I've never had a problem when doing it this way.