lpcware

LPC11C14 C_CAN on-chip drivers

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by mschuffe on Wed May 25 01:41:34 MST 2011
can everbody explain the setup of the mask into the CAN_MSG_OBJ

typedef struct _CAN_MSG_OBJ {
  uint32_t  mode_id;                        /* CAN idenifier*/         
  uint32_t  mask;                             /* setup for the mask ? */
  uint8_t   data[8];                          /* Data field */        
  uint8_t   dlc;                                 /* Length of data field in bytes DLC */  
  uint8_t   msgobj;                          /* Message object number 1-32*/     
}CAN_MSG_OBJ;


Thanks in advance,
Best Regards, Maik

Outcomes