Content originally posted in LPCWare by lpcxpresso-support on Thu Sep 17 04:40:27 MST 2015
Hi
First of all, just to give you confidence, we do, very regularly, test an LPC11U68 board on our own Linux Ubuntu 14.04 kit and it does normally work. I've just tried it manually too, with no problem.
As you know we don't test or support Linux Mint directly, but it seems reasonable to expect it to work if Ubuntu 14.04 does. The most frequent problems reported in this area are those to do with providing 32-bit libraries on 64-bit systems. Is yours a 32-bit or a 64-bit system? Have you checked the guidelines for installing under Linux contained in the LPCXpresso User Guide (available via your browser through Help).
The message you mention about "CMIS-DAP not found" is one that the IDE produces only when the a launch configuration has been established with a CMIS-DAP, otherwise it would report "No compatible emulators enabled" every time. Have you once had a successful CMIS-DAP debug connection? Or are these message appearing somewhere else (other than in the window that appears shortly after requesting to debug your project)?
I suggest that you delete the .launch files in your project to remove any previous setup information. (You can do this from the project explorer.)
There are a few logs available in the 'Console' panel. Do you think you could select those with names incorporating
* redlink server
* gdb traces
* arm-none-eabi-gdb
and include them in this thread.
Also, you have found that you can boot the debug probe OK with boot_link2, so do you think you could
* disconnect the LPC11U68
* wait a short while
* connect the LPC11U68
* run 'lsusb' and send us the output
* boot the debug probe
* run 'lsusb' and send us the output again
We're expecting an entry like
Bus 001 Device 012: ID 1fc9:000c NXP Semiconductors
to be in the first lsusb. And one like
Bus 001 Device 014: ID 1fc9:0090 NXP Semiconductors
to be in the second.
You mention that you have been successful in booting a Link1-attached device. Is this (and any other boards you may have) disconnected at the time when you have your failure? (It's best if they are.)
Sincerely,
LPCXpresso-Support