Content originally posted in LPCWare by MikeSimmonds on Thu Feb 21 20:53:31 MST 2013
[FONT=Tahoma][SIZE=1]Thanks, that did it, although I did not copy over a launch config ; I created one via the 'bug' icon on the toolbar.
When I do create a debug launch via the 'bug' icon, I can use it ok. BUT when I click debug in quick start, it totally
ignores any I have set up and makes a new one -- with all the wrong defaults for me.
Why is this?
(a) How can I get in and configure *BEFORE* the quickstart debug configuration runs for the first time?
(b) Why have you hidden the debug launch files (burried somewhere in .metadata IIRC) instead of leaving
them in the project directory (where some would argue that they belong -- are ther included in a project export?)
(c) The defaults are not what I want -- ever. Is there a way of setting a [I]workplace[/I] default debug configuration
so that every time I add a project (or I have to delete a launch config) I don't have to turn of red trace,
set no semi-hosting, select SWD, select no load, etc. etc.
Mike
[/SIZE][/FONT]