Content originally posted in LPCWare by IanJames on Tue Mar 12 07:15:49 MST 2013
Hi,
I am attempting to write a 512 byte variable to FLASH using the IAP routines.
The problem is I get an error code 2 [SRC_ADDR_ERROR]
I have looked in the map file and see that the address of the variable is 0x10000901 gNodeAddrTable
I assume this is the problem but how can I force the variable to to be word aligned?
I have another variable which works fine:
0x10000b12 gConfig
Thnaks,
Ian