Content originally posted in LPCWare by joaopeddro on Sat Oct 08 14:43:06 MST 2011
I have several questions to configure the pins as GPIO in lpcxpresso lpc1769,
a)I want turn on e turn off a LED that are physically connected to the lpcxpresso in pin P0.22. The datasheet of lpc1769 inform to put Pin P0.22 as output i need put 1 in the bits 12,13 an use register FIOD0, I did it this way : LPC_GPIO0->FIODIR0 = 0x0003000;
b)To turn off all the LEDs i did : LPC_GPIO0->FIOCLR0 = 0x0003000;
The problem is the Led don´t turn on.
The program is example GPIO :
#include <cr_section_macros.h>
#include <NXP/crp.h>
// Variable to store CRP value in. Will be placed automatically
// by the linker when "Enable Code Read Protect" selected.
// See crp.h header for more information
__CRP const unsigned int CRP_WORD = CRP_NO_CRP ;
#include "lpc17xx.h"
#include "type.h"
// Led 1 is P0_22
#define LED_2 (0 << 22)
int main (void)
{
uint32_t i, j;
/* SystemClockUpdate() updates the SystemFrequency variable */
SystemClockUpdate();
LPC_GPIO0->FIODIR0 = 0x0003000;/* P0.22 defined as Outputs */
LPC_GPIO0->FIOCLR0 = 0x0003000;/* turn off all the LEDs */
while(1)
{
for(i = 0; i < 8; i++)
{
LPC_GPIO0->FIOSET0 = 1 << i;
for(j = 1000000; j > 0; j--);
}
LPC_GPIO0->FIOCLR0 = 0x0003000;
for(j = 1000000; j > 0; j--);
}
}