Content originally posted in LPCWare by mstachowsky on Thu Oct 20 06:39:08 MST 2011
I'm trying to run this from the IDE by clicking on the flash button, maybe that is my issue? The command line options appear to be:
crt_emu_cm3_nxp -g -2 -pLPC1768 -flash-load-partial="C:\Users\Mike\Documents\LPCXpresso_4.1.0_190\workspace\uart\Debug\uart.axf" -wire=hid -s250
The output of the flash process log is:
Pc: ( 0) Reading remote configuration
Ni: LPCXpresso Debug Driver v4.0 (Sep 21 2011 20:05:40)
Nc: Looked for chip XML file in C:/nxp/LPCXpresso_4.1.0_190/lpcxpresso/bin/LPC1768.xml
Nc: Looked for vendor directory XML file in C:/nxp/LPCXpresso_4.1.0_190/lpcxpresso/bin/nxp_directory.xml
Nc: Found generic directory XML file in C:/nxp/LPCXpresso_4.1.0_190/lpcxpresso/bin/crt_directory.xml
Pc: ( 5) Remote configuration complete
Pc: ( 30) Emulator Connected
Pc: ( 40) Debug Halt
Pc: ( 50) CPU ID
Nc: Emu(0): Conn&Reset. DpID: 2BA01477. Info: T1S6RGRIA
Nc: SWD Frequency: 250 KHz. RTCK: False. Vector catch: False.
Nc: Packet delay: 0 Poll delay: 0.
Nc: NXP: LPC1768 Part ID: 0x26113F37
Pc: ( 65) Chip Setup Complete
'ipconfig.exe' is not recognized as an internal or external command,
operable program or batch file.
'cscript.exe' is not recognized as an internal or external command,
operable program or batch file.
Wt: License check failure (CheckLicense)
Nt: Connected: was_reset=false. was_stopped=true
Cr:f Restricted - unregistered license, download limit of 8K
Pc: ( 70) License Check Complete
Et:53: License does not permit flash operations from command line
Pc: (100) Target Connection Failed
I have a feeling that this has to do with the cscript problem mentioned in the link, so I'll give that a shot and see what the license diagnostic says.
Thanks for the help so far!
MIKE