lpcware

Reg:UART Library for  LPC1227

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by Microembedded on Thu May 15 06:04:47 MST 2014
From "I'm looking for a UART library for LPC1114"

i tried to post a message in the previous thread but my message was directed into spam.So i am reposting my message after creating a new thread.

I included the uart.c routine in my main file.This is how it looked like.

#ifdef __USE_CMSIS
#include "LPC122x.h"

#endif

#include <cr_section_macros.h>

#include <NXP/crp.h>
#include <type.h>
#include <gpio.h>
#include <string.h>
#include <uart.h>

/*****************************************************************************
** Function name:UART_IRQHandler
**
** Descriptions:UART interrupt handler
**
** parameters:None
** Returned value:None
**
*****************************************************************************/
void UART0_IRQHandler(void)
{
  uint8_t IIRValue, LSRValue;
  uint8_t Dummy = Dummy;

  IIRValue = LPC_UART0->IIR;

  IIRValue >>= 1;/* skip pending bit in IIR */
  IIRValue &= 0x07;/* check bit 1~3, interrupt identification */
  if (IIRValue == IIR_RLS)/* Receive Line Status */
  {
    LSRValue = LPC_UART0->LSR;
    /* Receive Line Status */
    if (LSRValue & (LSR_OE | LSR_PE | LSR_FE | LSR_RXFE | LSR_BI))
    {
      /* There are errors or break interrupt */
      /* Read LSR will clear the interrupt */
      UARTStatus0 = LSRValue;
      Dummy = LPC_UART0->RBR;/* Dummy read on RX to clear
interrupt, then bail out */
      return;
    }
    if (LSRValue & LSR_RDR)/* Receive Data Ready */
    {
      /* If no error on RLS, normal ready, save into the data buffer. */
      /* Note: read RBR will clear the interrupt */
      UARTBuffer0[UARTCount0++] = LPC_UART0->RBR;
      if (UARTCount0 == BUFFSIZE)
      {
        UARTCount0 = 0;/* buffer overflow */
      }
    }
  }
  else if (IIRValue == IIR_RDA)/* Receive Data Available */
  {
    /* Receive Data Available */
    UARTBuffer0[UARTCount0++] = LPC_UART0->RBR;
    if (UARTCount0 == BUFFSIZE)
    {
      UARTCount0 = 0;/* buffer overflow */
    }
  }
  else if (IIRValue == IIR_CTI)/* Character timeout indicator */
  {
    /* Character Time-out indicator */
    UARTStatus0 |= 0x100;/* Bit 9 as the CTI error */
  }
  else if (IIRValue == IIR_THRE)/* THRE, transmit holding register empty */
  {
    /* THRE interrupt */
    LSRValue = LPC_UART0->LSR;/* Check status in the LSR to see if
valid data in U0THR or not */
    if (LSRValue & LSR_THRE)
    {
      UARTTxEmpty0 = 1;
    }
    else
    {
      UARTTxEmpty0 = 0;
    }
  }
  return;
}

/*****************************************************************************
** Function name:UART_IRQHandler
**
** Descriptions:UART interrupt handler
**
** parameters:None
** Returned value:None
**
*****************************************************************************/
void UART1_IRQHandler(void)
{
  uint8_t IIRValue, LSRValue;
  uint8_t Dummy = Dummy;

  IIRValue = LPC_UART1->IIR;

  IIRValue >>= 1;/* skip pending bit in IIR */
  IIRValue &= 0x07;/* check bit 1~3, interrupt identification */
  if (IIRValue == IIR_RLS)/* Receive Line Status */
  {
    LSRValue = LPC_UART1->LSR;
    /* Receive Line Status */
    if (LSRValue & (LSR_OE | LSR_PE | LSR_FE | LSR_RXFE | LSR_BI))
    {
      /* There are errors or break interrupt */
      /* Read LSR will clear the interrupt */
      UARTStatus1 = LSRValue;
      Dummy = LPC_UART1->RBR;/* Dummy read on RX to clear
interrupt, then bail out */
      return;
    }
    if (LSRValue & LSR_RDR)/* Receive Data Ready */
    {
      /* If no error on RLS, normal ready, save into the data buffer. */
      /* Note: read RBR will clear the interrupt */
      UARTBuffer1[UARTCount1++] = LPC_UART1->RBR;
      if (UARTCount1 == BUFFSIZE)
      {
        UARTCount1 = 0;/* buffer overflow */
      }
    }
  }
  else if (IIRValue == IIR_RDA)/* Receive Data Available */
  {
    /* Receive Data Available */
    UARTBuffer1[UARTCount1++] = LPC_UART1->RBR;
    if (UARTCount1 == BUFFSIZE)
    {
      UARTCount1 = 0;/* buffer overflow */
    }
  }
  else if (IIRValue == IIR_CTI)/* Character timeout indicator */
  {
    /* Character Time-out indicator */
    UARTStatus1 |= 0x100;/* Bit 9 as the CTI error */
  }
  else if (IIRValue == IIR_THRE)/* THRE, transmit holding register empty */
  {
    /* THRE interrupt */
    LSRValue = LPC_UART1->LSR;/* Check status in the LSR to see if
valid data in U0THR or not */
    if (LSRValue & LSR_THRE)
    {
      UARTTxEmpty1 = 1;
    }
    else
    {
      UARTTxEmpty1 = 0;
    }
  }
  return;
}

/*****************************************************************************
** Function name:ModemInit
**
** Descriptions:Initialize UART0 port as modem, setup pin select.
**
** parameters:location
** Returned value:None
**
*****************************************************************************/
void ModemInit( uint32_t location )
{
  if ( location == 0 )
  {
LPC_IOCON->PIO0_3 &= ~0x07;    /* UART I/O config */
LPC_IOCON->PIO0_3 |= 0x02;     /* UART DTR output */
LPC_IOCON->PIO0_7 &= ~0x07;
LPC_IOCON->PIO0_7 |= 0x02;     /* UART CTS input */
LPC_IOCON->PIO0_0 &= ~0x07;
LPC_IOCON->PIO0_0 |= 0x02;     /* UART RTS output */
LPC_IOCON->PIO0_4 &= ~0x07;
LPC_IOCON->PIO0_4 |= 0x02;     /* UART DSR input */
LPC_IOCON->PIO0_5 &= ~0x07;
LPC_IOCON->PIO0_5 |= 0x02;     /* UART DCD input */
LPC_IOCON->PIO0_6 &= ~0x07;
LPC_IOCON->PIO0_6 |= 0x02;     /* UART RI input */
  }
  else if ( location == 1 )
  {
LPC_IOCON->PIO2_3 &= ~0x07;    /* UART I/O config */
LPC_IOCON->PIO2_3 |= 0x04;     /* UART DTR output */
LPC_IOCON->PIO2_4 &= ~0x07;
LPC_IOCON->PIO2_4 |= 0x04;     /* UART CTS input */
LPC_IOCON->PIO2_0 &= ~0x07;
LPC_IOCON->PIO2_0 |= 0x04;     /* UART RTS output */
LPC_IOCON->PIO2_7 &= ~0x07;
LPC_IOCON->PIO2_7 |= 0x04;     /* UART DSR input */
LPC_IOCON->PIO2_6 &= ~0x07;
LPC_IOCON->PIO2_6 |= 0x04;     /* UART DCD input */
LPC_IOCON->PIO2_5 &= ~0x07;
LPC_IOCON->PIO2_5 |= 0x04;     /* UART RI input */
  }
  LPC_UART0->MCR = 0xC0;          /* Enable Auto RTS and Auto CTS. */
  return;
}

/*****************************************************************************
** Function name:SetupUART_Location
**
** Descriptions:Setup UART0 location
**
** parameters:port number, location
** Returned value:None
**
*****************************************************************************/
void SetupUART_Location(uint32_t portNum, uint32_t location)
{
  if ( portNum == 0 )
  {
if ( location == 0 )
{
  LPC_IOCON->PIO0_1 &= ~0x07;    /* UART0 I/O config */
  LPC_IOCON->PIO0_1 |= 0x02;     /* UART0 RXD LOC0 */
  LPC_IOCON->PIO0_2 &= ~0x07;
  LPC_IOCON->PIO0_2 |= 0x02;     /* UART0 TXD LOC0 */
}
else if ( location == 1 )
{
  LPC_IOCON->PIO2_1 &= ~0x07;    /* UART0 I/O config */
  LPC_IOCON->PIO2_1 |= 0x04;     /* UART0 RXD LOC1 */
  LPC_IOCON->PIO2_2 &= ~0x07;
  LPC_IOCON->PIO2_2 |= 0x04;     /* UART0 TXD LOC1 */
}
  }
  else if ( portNum == 1 )
  {
if ( location == 0 )
{
  LPC_IOCON->PIO0_8 &= ~0x07;    /* UART1 I/O config */
  LPC_IOCON->PIO0_8 |= 0x02;     /* UART1 RXD LOC0 */
  LPC_IOCON->PIO0_9 &= ~0x07;
  LPC_IOCON->PIO0_9 |= 0x02;     /* UART1 TXD LOC0 */
}
else if ( location == 1 )
{
  LPC_IOCON->PIO2_11 &= ~0x07;    /* UART1 I/O config */
  LPC_IOCON->PIO2_11 |= 0x05;     /* UART RXD LOC1 */
  LPC_IOCON->PIO2_10 &= ~0x07;
  LPC_IOCON->PIO2_10 |= 0x05;     /* UART TXD LOC1 */
}
else
{
  LPC_IOCON->PIO2_12 &= ~0x07;    /* UART1 I/O config */
  LPC_IOCON->PIO2_12 |= 0x03;     /* UART RXD LOC1 */
  LPC_IOCON->PIO2_13 &= ~0x07;
  LPC_IOCON->PIO2_13 |= 0x03;     /* UART TXD LOC1 */
}
  }
  else
  {
while ( 1 );
  }
  return;
}

/*****************************************************************************
** Function name:UARTInit
**
** Descriptions:Initialize UARTx port, setup pin select,
**clock, parity, stop bits, FIFO, etc.
**
** parameters:UART port number, baudrate
** Returned value:None
**
*****************************************************************************/
void UARTInit(uint32_t portNum, uint32_t baudrate)
{
  uint32_t i, Fdiv;
  uint32_t regVal;

  if ( portNum == 0 )
  {
UARTTxEmpty0 = 1;
UARTCount0 = 0;
    for ( i = 0; i < BUFFSIZE; i++ )
{
  UARTBuffer0 = 0;
}
NVIC_DisableIRQ(UART0_IRQn);

SetupUART_Location( portNum, 0 );/* default is location 0 */

/* Enable UART 0 clock */
LPC_SYSCON->PRESETCTRL |= (0x1<<2);
LPC_SYSCON->SYSAHBCLKCTRL |= (0x1<<12);
LPC_SYSCON->UART0CLKDIV = 0x1;     /* divided by 1 */

LPC_UART0->LCR = 0x83;             /* 8 bits, no Parity, 1 Stop bit */
regVal = LPC_SYSCON->UART0CLKDIV;
Fdiv = ((SystemCoreClock/regVal)/16)/baudrate ;/*baud rate */ //16

//LPC_UART0->DLM = Fdiv / 256;
LPC_UART0->DLM = 0x00;
//LPC_UART0->DLL = Fdiv % 256;
LPC_UART0->DLL = 0x16;
LPC_UART0->LCR = 0x03;/* DLAB = 0 */
LPC_UART0->FDR = 0x10;/* set to default value: 0x10 *///0x10
LPC_UART0->FCR = 0x07;/* Enable and reset TX and RX FIFO. */

/* Read to clear the line status. */
regVal = LPC_UART0->LSR;

/* Ensure a clean start, no data in either TX or RX FIFO. */
while ( (LPC_UART0->LSR & (LSR_THRE|LSR_TEMT)) != (LSR_THRE|LSR_TEMT) );
while ( LPC_UART0->LSR & LSR_RDR )
{
  regVal = LPC_UART0->RBR;/* Dump data from RX FIFO */
}

/* Enable the UART Interrupt */
NVIC_EnableIRQ(UART0_IRQn);

#if TX_INTERRUPT
LPC_UART0->IER = IER_RBR | IER_THRE | IER_RLS;/* Enable UART interrupt */
#else
LPC_UART0->IER = IER_RBR | IER_RLS;/* Enable UART interrupt */
#endif
  }
  else
  {
UARTTxEmpty1 = 1;
UARTCount1 = 0;
    for ( i = 0; i < BUFFSIZE; i++ )
{
  UARTBuffer1 = 0;
}
NVIC_DisableIRQ(UART1_IRQn);

SetupUART_Location( portNum, 0 );/* default is location 0 */

/* Enable UART 1 clock */
LPC_SYSCON->PRESETCTRL |= (0x1<<3);
LPC_SYSCON->SYSAHBCLKCTRL |= (0x1<<13);
LPC_SYSCON->UART1CLKDIV = 0x1;     /* divided by 1 */

LPC_UART1->LCR = 0x83;             /* 8 bits, no Parity, 1 Stop bit */
regVal = LPC_SYSCON->UART1CLKDIV;
Fdiv = ((SystemCoreClock/regVal)/12)/baudrate ;/*baud rate */

LPC_UART1->DLM = Fdiv / 256;
LPC_UART1->DLL = Fdiv % 256;
LPC_UART1->LCR = 0x03;/* DLAB = 0 */
LPC_UART1->FDR = 0x10;/* set to default value: 0x10 */
LPC_UART1->FCR = 0x07;/* Enable and reset TX and RX FIFO. */

/* Read to clear the line status. */
regVal = LPC_UART1->LSR;

/* Ensure a clean start, no data in either TX or RX FIFO. */
while ( (LPC_UART1->LSR & (LSR_THRE|LSR_TEMT)) != (LSR_THRE|LSR_TEMT) );
while ( LPC_UART1->LSR & LSR_RDR )
{
  regVal = LPC_UART1->RBR;/* Dump data from RX FIFO */
}

/* Enable the UART Interrupt */
NVIC_EnableIRQ(UART1_IRQn);

#if TX_INTERRUPT
LPC_UART1->IER = IER_RBR | IER_THRE | IER_RLS;/* Enable UART interrupt */
#else
LPC_UART1->IER = IER_RBR | IER_RLS;/* Enable UART interrupt */
#endif
  }
  return;
}

/*****************************************************************************
** Function name:UARTSend
**
** Descriptions:Send a block of data to the UART 0 port based
**on the data length
**
** parameters:portNum, buffer pointer, and data length
** Returned value:None
**
*****************************************************************************/
void UARTSend(uint32_t portNum, uint8_t *BufferPtr, uint32_t Length)
{

  while ( Length != 0 )
  {
if ( portNum == 0 )
{
  /* THRE status, contain valid data */
#if !TX_INTERRUPT
  while ( !(LPC_UART0->LSR & LSR_THRE) );
  LPC_UART0->THR = *BufferPtr;
#else
  /* Below flag is set inside the interrupt handler when THRE occurs. */
      while ( !(UARTTxEmpty0 & 0x01) );
  LPC_UART0->THR = *BufferPtr;
      UARTTxEmpty0 = 0;/* not empty in the THR until it shifts out */
#endif
}
else
{
  /* THRE status, contain valid data */
#if !TX_INTERRUPT
  while ( !(LPC_UART1->LSR & LSR_THRE) );
  LPC_UART1->THR = *BufferPtr;
#else
  /* Below flag is set inside the interrupt handler when THRE occurs. */
      while ( !(UARTTxEmpty1 & 0x01) );
  LPC_UART1->THR = *BufferPtr;
      UARTTxEmpty1 = 0;/* not empty in the THR until it shifts out */
#endif
}
BufferPtr++;
Length--;
  }
  return;
}
int main (void)
    {

           SetupUART_Location(0,0);
           UARTInit(0, 9600);
            while(1)
        {
            if ( UARTCount0 != 0 )
                {
                  LPC_UART0->IER = IER_THRE | IER_RLS;                      /* Disable RBR */
                  UARTSend( 0, "UARTONDONEOK" , 12);
            
            
                  UARTCount0 = 0;
                  LPC_UART0->IER = IER_THRE | IER_RLS | IER_RBR;    /* Re-enable RBR */
               }
         }
}

If i run this program I am getting junk data in my terminal.If i increase the character length,length of junk data too increases.I am using 12MHz clock.I suspect baudrate type issue.

Please check if i  have gone wrong somewhere.

Thanks a lot.

Outcomes