LPCXpresso 1769 -- JVM_Bind

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCXpresso 1769 -- JVM_Bind

172 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by icietla on Wed Nov 07 13:12:28 MST 2012
As I was experimenting with some simple code, all was going well until I got the following message:
"Connecting to target: StubMsgServer:Address already in use:JVM_Bind"

There are a number of post on the Internet saying that this is cause by the "port" still being in use by a previous session.
What I did:
Unplug the LCPXpresso Board and retry:
No Change.
Close the LPCXpresso software and re-start.
No change.
Reboot Windows 7:
No change.

I'm lost as what to do next.  It was working before and no changes were made (knowingly) to the Windows environment.

I would appreciate some pointers on what should be my next steps.

Thanks
Normand
0 Kudos
1 Reply

163 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by icietla on Thu Nov 08 07:57:49 MST 2012
Finally I did reinstall the LPCXpresso environment after cleaning all traces of it from my computer.
It now works but I still have no idea of what caused the problem.
0 Kudos