Content originally posted in LPCWare by fjrg76 on Thu Nov 03 23:29:30 MST 2011
NXP LPC1114 drivers are far to be useful.
Let's see at the UART's driver. As it is written, the only parameter you can configure is the baudrate. Data bits, parity and stop bits are fixed. In the case you need some other configuration you must re-write the init_uart() function. Even more, the driver doesn't include a uart_get_char() function.
While writing my timer's driver I realized that it has at least 7 parameters that can be configured, and the included driver only has 3.
These drivers should be used as an entry point for our own drivers. In this case (I guess) the license has not effects, right?
Greetings.